OSRAM SFH 4718A OSLON Black IR LED Now at Mouser Electronics for Hi-Res Security Camera Applications
September 6, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the SFH 4718A infrared LED (IRED), part of the IR OSLON Black family from OSRAM Opto Semiconductors. The small but powerful IRED is the first in the family to feature a narrow beam angle of ± 25 degrees, enabling illumination units for camera systems with a medium capture range without requiring secondary optics.
With the OSRAM SFH 4718A IRED, now available from Mouser Electronics, the OSLON Black portfolio now comprises three wavelengths (810 nm, 850 nm and 940 nm) and three beam angles (±25, ±45 and ±75 degrees), with optical outputs ranging from 0.3 W to 2 W. The SFH 4718A offers an optical output of 0.8 W at 1 A, and an excellent radiant intensity of 730 W/sr. The device's 850 nm wavelength is barely discernible by humans, but lies within the sensitivity range of the camera sensors.
OSRAM OSLON Black SFH 4718A IREDs come in a small 3.75 × 3.75 mm package with a low thermal resistance of 16 K/W (max) and electrostatic discharge (ESD) protection to 2 kV. The device is ideal for a range of security and recognition applications, including 3D image capture and facial-scan access control. Engineers can also use the IREDs in systems to illuminate areas monitored by closed-circuit television (CCTV) systems, as well as for automatic license plate recognition systems.
To learn more, visit www.mouser.com/osram-sfh-4718-oslon-black-led.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About OSRAM Opto Semiconductors
OSRAM Opto Semiconductors is a world leading manufacturer of optoelectronic semiconductors for the lighting, sensor, and visualization sectors. The extensive product portfolio of OSRAM Opto Semiconductors includes a wide selection of high-brightness high-power LEDs in the visible range along with other semiconductor technologies used in a variety of lighting applications.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com