Now at Mouser: Transphorm's 4kW Analog-Controlled Bridgeless Totem-Pole PFC Board
September 17, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the 4kW Analog Bridgeless Totem-Pole PFC Board from Transphorm.
Transphorm 4kW Analog Bridgeless Totem-Pole Power Factor Correction (PFC) Board (TDTTP4000W065AN) achieves very high efficiency single-phase AC-DC conversion using the TP65H035WSG4, a diode-free Gallium Nitride (GaN) FET bridge with low reverse-recovery charge. Using the Transphorm GaN FETs in the fast-switching leg of the circuit and low-resistance MOSFETs in the slow-switching leg of the circuit results in improved performance and efficiency.
The TP65H035G4WS MOSFET is a normally-off device that enables the AC-DC bridgeless totem-pole PFC designs. The MOSFET features fast-switching leg and low-resistance Silicon MOSFETs in the slow-switching leg of the circuit. This TP65H035G4WS MOSFET device is designed with the latest Gen IV SuperGaN™ technology.
The TDTTP4000W065AN board uses the bridgeless totem-pole power factor correction (PFC) topology with a traditional Texas Instruments UCC28180 analog controller. This pairing provides fast and easy access to the high power density made possible by GaN FETs without the need for firmware development required by DSP. This board operates from 85V to 265V AC input voltage range and 387V DC output voltage.
Typical applications include data center and industrial power supplies.
To learn more, visit https://www.mouser.com/new/transphorm/transphorm-tdttp4000w065an-eval-board/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 800 manufacturers. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com