Ethernet Protection for Exposed Data Lines
Image Source: xiaoliangge -
stock.adobe.com
By Kelly Casey, Mouser Electronics
Published January 14, 2020
Engineers are being asked to connect absolutely everything to a network. The network protocol of choice is
Ethernet or one of the myriad variations. Some of these assignments can look great on paper but suffer serious
setbacks in the modern world.
The original designers of the Ethernet could not have imagined what we have done with their "baby", whose
original intent was to connect various computers together at a data rate of 10Mbps, which was fast enough for
the processors in the computers they were using at the time. The computers were all located in a single room or
data center, the computer cables could be no longer than 10m, and conditions in that data room were controlled
so that electrostatic discharge (ESD) was a minimal threat. Once the computers were wired in, they stayed
physically connected for very long periods.
Today, we regularly run Gigabit Ethernet— or at least 100Base-T over hundreds of meters. The buildings we
work and live in have miles of cables buried in their walls and ceilings. We use Power over Ethernet (PoE) to
power as well as communicate with devices located on rooftops, in kiosks, on light poles, and even radio towers.
When the boss tells you to replace the IEEE-488 links in the factory with Ethernet, he/she may not understand
the inherent robustness of the IEEE-488 link and the engineering you will need to do to keep your new Ethernet
network up and running in an industrial environment. You will need a network circuit protection scheme that will
provide trouble-free service for years, and hope it is not a scheme!
To be fair, the vast majority of Ethernet runs require no special protection. The first electrical component
behind most RJ-45 Ethernet jacks is an isolation transformer that will provide some protection. This, paired
with the ESD protection built into most Ethernet physical layer (PHY) transceiver IC's, provides adequate
protection in most home and office environments. The problem is the low percentage of Ethernet ports that are
exposed to more serious threats. Long cable runs inside buildings become long-wire antennae that can couple
energy from nearby lightning strikes into the network. Those “antennae” are even better at collecting lightning
energy if they are run outdoors to kiosks or up to rooftop or pole-top security cameras.
When reliability issues first surfaced, ciruit protection companies developed protection "dongles" that provided
additional ESD overvoltage protection. At the time, the dongle plugged into the troubled RJ-45 jack and provided
a "protected" RJ-45 jack of its own. These were added to the routers or other equipment that was experiencing
failures and were effective up to a point.
As data rates climb and with the advent of PoE, custom solutions are needed and the "one-size-fits-all" dongle
approach is often inadequate. PoE brings on even more issues as the direct current (DC) voltages present can
trip the overvoltage protection in dongles designed only for the 2V Ethernet signal. Gigabit data rates can
suffer significant data errors due to the capacitive loading of protection schemes designed for 10Base-T or
100Base-T networks.
Unlike 10Base-T, Gigabit Ethernet uses a complex coding scheme (Figure 1) that requires a very
linear channel to
successfully propagate long distances. Silicon diodes and thyristors exhibit a non-linear capacitance dependence
on the applied voltage. Gigabit Ethernet also uses a clock rate more than ten times faster than 10-BaseT, which
makes the signal more sensitive to the capacitance of the cable and any protection devices used.
Building a robust Ethernet network usually requires a "layered" approach consisting of Primary, Secondary and,
sometimes, Tertiary layers. Each layer performs a specific task.
Primary Layer: Borrowing technology developed for telecommunications outside plant applications,
gas discharge tubes (GDT's), such as the EPCOS/TDK T83-A90X, can provide the needed surge-handling capabilities with minimal capacitance
loading. The primary layer will let through voltages that are still too high, though it limits the duration of
the surge as most of the energy is shunted to ground. For PoE applications, the breakdown voltage of the
protection devices must be higher than the PoE power supply voltage. Also, the design engineer must assure that
the primary protection system will "delatch" or "reset" while connected to the power supply after the protection
is activated. Often, this requires a fold-back current limited PoE supply and protection devices with high
holding currents.
Secondary Layer: The isolation transformers not only provide DC isolation to the PHY transceiver
IC, their tiny magnetic cores easily saturate and limit the amount of energy that is coupled into the
transceiver circuit. However, isolation between the windings must be able to withstand the let-through voltages
of the primary layer without breaking down. Keep in mind that a GDT may have a DC breakdown voltage of 90V, but
may overshoot to as high as 500V under fast dv/dt lightning surge conditions. The inter-winding capacitance can
also couple energy across the isolation barrier, but this is usually quite small compared with the magnetically
coupled energy.
Tertiary Layer: The primary and secondary protectors have removed the PoE power and limited the
maximum voltage and current to levels that can be managed by a wide range of technologies, many of which borrow
technology from ESD protection devices. Some examples:
- Differential overvoltage protection, such as that provided by a STMicroelectronics SLVU2.8 in the Standard
Product series, is a simple and elegent solution, but provides no protection from energy coupled
through the transformer inter-winding capacitance. This is often an acceptable solution.
- ON Semiconductor's ESD Protection Diodes & Arrays product series offers longitudinal grounded
protection for the inter-winding capacitance let-through energy.
- Bourns offers TCS™ DL High-Speed Protectors
Series devices that protect by limiting the maximum current in the PHY transceiver inputs and
outputs to a safe level rather than the overvoltage scheme of shunting the current around the protected
load. These can only handle 40V, so well-layered protection is a must for exposed Ethernet.
Figure 1: Gigabit Ethernet uses a complex coding scheme (Source: Mouser
Electronics)
Today's demanding Ethernet applications go far beyond the scope of the original ethernet concept in distances,
data rates, and exposure to surge threats. With careful engineering, robust Ethernet networks can be deployed
into very challenging environemnts.
Kelly Casey is VP of Engineering for
FM
Technical Consulting, and holds a Bachelor of Science Degree in Electrical Engineering from the University
of Nebraska,
as well as a Master of Science Degree in Electrical Engineering from the Georgia Institute of Technology.
Previously,
Mr. Casey has held various roles at Bourns, Littelfuse, and Teccor Electronics.