Air-Quality Sensors: Redefining Environmental Sensing
By Bill Schweber for Mouser Electronics
There has always been a widespread need for electronic sensors that can handle a diverse range of
physical phenomena, such as light, pressure, sound, and, of course, temperature (the most widely sensed parameter).
The good news is that there have been significant advances in delivering high-performance, low-cost, easy-to-use
sensors for many of these measurements, with progress often based on microelectromechanical systems (MEMS) technology. For example, sensing of position
and motion—two closely related physical attributes that are traditionally among the most challenging to
measure—is now almost trivial due to the widespread availability of tiny silicon-based accelerometers and
gyroscopes, which are widely used for navigation in drones and for car safety.
Still, one sensing area has long eluded the development of high-performance, low-cost, low-power sensors: vapor and
gas (smell) sensing. We are still a long way from a sensitive, universal odor-sniffing capacity equating that of a
beagle’s or even a human’s nose. Sensors for gases, volatile organic compounds (VOCs), and even humidity
have been especially challenging to develop, and they have been harder to use, calibrate, and integrate than
temperature sensors. Further, each gas sensor often has a different analog output format that involves scaling,
voltage versus current, timing, and other variations (Figure 1).
Figure 1: Different analog interfaces are commonly used for sensors, including
the three-wire voltage, four-wire voltage, and two-wire 4mA to 20mA current outputs. Integrating a set of
different sensors can become a challenge for analog input/output (I/O). (Source: TE)
The problem is aggravated when it is necessary to measure multiple, distinct variables at a single location. Simply
and successfully interfacing with the diverse variety of available sensing solutions requires limiting sensor
choices, adding adapter circuits to yield a single output format, or interfacing with multiple output formats.
Throughout the last decade, though, there has been significant progress, as MEMS and associated semiconductors have
been radically changing the situation and providing low-power, low-cost sensors for specific gases. However,
these advances began with application-specific impact and pressure sensors for air bag triggering, as opposed to
with gas sensors. This research, development, and commercialization has opened the way for progress in MEMS sensors
regarding pressure, VOCs, and carbon dioxide (CO2). The result has created widespread availability of
microchip-based devices for basic sensing of gases and liquids as well as for calibration, additional integrated
features, and more embedded functions.
Trend: Single-Point, Multi-Factor Sensing
As sensors have advanced in terms of their basic performance, ease of interconnect, cost, and power requirements,
there has been a corresponding trend of sensing multiple parameters at each location. This is a departure from
previous architectures where only temperature (and perhaps humidity) were sensed and measured at one location, and
VOCs and CO2 were sensed at another, for example. With the newer sensors, it is feasible and actually
makes sense to integrate a full set of sensors at each site with single-path (wired or wireless) connectivity.
Doing so serves various applications that need sensor data across multiple parameters. These include lighting control, building automation, security, motion and presence sensing, smart homes,
connected homes, air quality monitoring, and energy management. Further, by combining the full roster of desired
sensors into a single device, system designers, their projects, and even the end-users benefit from a reduced time
to market, fewer design “surprises,” and reduced installation costs, because designers no longer need to
deal with individual sensors and interfaces (unless they need to or want to do so). This enables low-cost,
convenient placement of multifunctional environmental-sensor nodes in industrial, commercial, institutional, and
residential settings.
Leveraging this new multisensory opportunity, vendors have developed small boards and modules that offer a
selection of commonly needed sensing functions, as complete, highly integrated, calibrated, and easy-to-use
solutions for these applications. Two products demonstrate how change in the integrated sensing of multiple physical
variables, including gas-based variables, is greatly simplifying challenges as well as opening new opportunities.
These include the:
TE Connectivity AmbiMate Sensor Module MS4 Series
This unit from TE Connectivity targets fixed-in-place
installations, such as buildings, and is packaged on a PC board that measures a mere 16mm × 30mm
(Figure 2). TE
Connectivity’s AmbiMate Sensor Module MS4 Series enables the sensing of well-known environmental and
presence parameters of motion via a passive infrared (PIR) detector, light, temperature, and humidity. It also
offers optional microphone-based sound detection, VOC sensing for ambient air quality and hazardous conditions, and
CO2 sensing (Figure 3).
Figure 2: The AmbiMate Sensor Module from TE Connectivity is a small PC board
intended for fixed installations. (Source: Mouser)
Figure 3: The AmbiMate Sensor Module board is housed in a user-provided
enclosure. Included on the board are sensors for (1) temperature; (2) relative humidity; (3) motion; (4) ambient
light; (5) audio microphone (optional); (6) VOCs (optional); and (7) CO2 (optional). (Source: Mouser)
The AmbiMate Sensor Module operates from a single 3.3VDC supply (which is nominal, with a 3.1V minimum) and
requires just 10mA (or 33mA with the VOC/CO2 sensing option) for low dissipation, high reliability, and
long operating life from a local battery. Accuracy for the temperature reading is ±0.3°C from 5°C to
50°C, while the accuracy of its humidity reading over the five percent to ninety-five percent relative humidity
(RH) range is two percent. Both temperature and humidity sensors have 1s update rates.
For the gas sensing functions, the unit can handle VOCs with concentrations from 0 to 1,187 parts per billion (ppb)
and CO2 readings from 400 to 8,192 parts per million (ppm). Both gas-related readings have 60s
acquisition periods.
The module can be queried at any time via its 100kbaud inter-integrated circuit (I2C) interface, and it
also includes an interrupt-driven event pin for motion- and sound-level detection, with a response time under 0.5s.
The audio-alarm output has a sensitivity of between -25dBV and -19dBV over a frequency range of 100Hz to 10kHz.
Bosch Sensortec BME680 Integrated Environmental Sensor
In contrast to the AmbiMate module, the Bosch Sensortec BME680 Integrated
Environmental Sensor
unit integrates high-linearity and high-accuracy gas, pressure, humidity, and temperature sensors in a package
developed specifically for mobile applications and wearable devices. The tiny metal-lid land grid array (LGA)
enclosure has a 3mm × 3mm footprint and is just 0.95mm high (Figure 4). To ease interfacing
with different processor configurations, it supports one I2C and two serial peripheral interface (SPI)
I/O formats (Figure 5).
Figure 4: The Bosch Sensortec BME680 Integrated Environmental Sensor for
mobile and wearable devices is a nearly invisible 3mm × 3mm metal-lid device, yet it includes an array of sensors,
calibration, and I/O functions within the enclosure. (Source: Bosch)
Figure 5: To facilitate connectivity between the BME680 and its host
processor, the unit includes the three commonly used low-power options, which are the: (a) I2C interface; (b)
four-wire SPI; and (c) three-wire SPI. (Source: Mouser)
The BME680 is well suited for sensing VOCs in paints, lacquers, paint strippers, office equipment, glues,
adhesives, and alcohol. It includes embedded calibration, and in addition to ethanol, the sensors also test exhaled
human breath for VOCs and important compounds (Table 1).
Table 1: The detailed data sheet for the BME680 includes a table of its tolerance and accuracy
when sensing the most-common VOCs. (Source: Bosch)
|
Molar Fraction
|
Compound
|
Production Tolerance
|
Certified Accuracy
|
|
5ppm
|
Ethane
|
20%
|
5%
|
|
10ppm
|
Isoprene (a.k.a., 2-Methyl-1,3 Butadiene)
|
20%
|
5%
|
|
10ppm
|
Ethanol
|
20%
|
5%
|
|
50ppm
|
Acetone
|
20%
|
5%
|
|
15ppm
|
Carbon Monoxide
|
10%
|
2%
|
The gas-sensing function of the BME680 demonstrates the level of integration and
sophistication that is embedded in this miniscule device. This function involves two steps:
- An integral gas-sensor hot plate is heated to a target temperature, typically between 200°C and 400°C,
and sustained for a required time period.
- The resistance of the gas-sensitive layer of the sensor is measured, and this resistance value is then mapped to
a corresponding value of VOC concentration.
In developing this device, every effort was made to minimize power consumption—a critical parameter for
mobile and wearable applications. Therefore, the device operates from a 1.71V to 3.6V supply. Current requirements
are in the single-digit microamp range for each sensor (1Hz update rate), with an increase to about 12mA for the
active gas-sensor mode; quiescent current is miserly at under 0.1mA in ultra-low-power mode and 0.15μA in sleep
mode.
Conclusion
There is no longer a need for original equipment manufacturers (OEMs) to identify, buy, mechanically and
electrically integrate, and code multiple sensors from different sources. Highly integrated MEMS and semiconductor
devices enable placement of multiple sensors for different physical variables in a single, tiny, low-power package.
Even the challenge of sensing VOCs and CO2 has been largely overcome due to these technological advances.
Sensor and system performance is assured and known (as these devices come with detailed specifications), circuit
interfacing is greatly simplified, and system integration is streamlined via software drivers and tools.
Bill Schweber is a contributing writer for Mouser Electronics and an electronics engineer who has written three textbooks on electronic
communications systems, as well as hundreds of technical articles, opinion columns, and product features. In past
roles, he worked as a technical web-site manager for multiple topic-specific sites for EE Times , as well as both
the Executive Editor and Analog Editor at EDN.
At Analog Devices, Inc. (a leading vendor of analog and
mixed-signal ICs), Bill was in marketing communications (public relations); as a result, he has been on both sides
of the technical PR function, presenting company products, stories, and messages to the media and also as the
recipient of these.
Prior to the MarCom role at Analog, Bill was associate editor of their respected technical
journal, and also worked in their product marketing and applications engineering groups. Before those roles, Bill
was at Instron Corp., doing hands-on analog- and power-circuit design and systems integration for materials-testing
machine controls.
He has an MSEE (Univ. of Mass) and BSEE (Columbia Univ.), is a Registered Professional
Engineer, and holds an Advanced Class amateur radio license. Bill has also planned, written, and presented on-line
courses on a variety of engineering topics, including MOSFET basics, ADC selection, and driving LEDs.