Advancing power supply solutions through the promise of GaN
By Texas Instruments
"Achieving more efficient electrical power conversion is a key technical goal in a world with a growing
population and an ever-expanding need for energy."
One important innovation that promises to contribute significantly to meeting this goal is the use of
gallium-nitride (GaN) in power applications. GaN is already an established semiconductor material, employed
extensively in LED lighting and increasingly important in wireless applications. Now, with process advances and
defect rate improvements, GaN is providing a number of advantages in electronic power supplies that convert
electricity between alternating and direct current, change voltage levels and perform a number of functions to
ensure the availability of reliable electric power.
The GaN-based switching power transistors that enable new power applications can operate at high voltages with
much higher performance
and lower losses than previously used silicon (Si) transistors. GaN characteristics, such as high-frequency
operation, promote high performance while maintaining high efficiency. The GaN devices use a GaN-on-Si process
that fits into the existing Si manufacturing flow. Given the much smaller size of the GaN device for the same
current capabilities, the GaN transistor should eventually be as cost effective as its Si equivalent. This will
make GaN devices attractive for systems ranging from huge industrial equipment to the smallest handheld devices.
GaN will find its first home in higher-performance power designs because of its benefits. These designs are
demanding as they push their operating frequencies and require precise switching characteristics. However, the
promise of GaN for more efficient power conversion is steadily coming within reach.
Today, power supply designers are beginning to rethink their circuits, looking for ways to create power systems
that can take full advantage of the new GaN transistors' potential, while avoiding unwanted effects. When
considerations like these enter the picture, solutions are often found in the components themselves-GaN
switches, Si switch drivers, high-speed switching controllers, and the power inductors, transformers and
capacitors that are part of the overall design. Integrated circuit (IC) manufacturers who create power products
can enhance the design possibilities considerably for customers by providing system-level solutions with
co-designed devices, even to the point of integrating multiple chips in modular packages.
Texas Instruments (TI), the industry leader in IC solutions for power applications, is well-positioned to provide
these types of solutions. With its innovative manufacturing processes, circuitry and packaging technologies, TI
continues to supply devices that enable designers to get the most out of GaN.
GaN's place in the power supply chain
Most familiar electronic equipment operates from switched-mode power supplies (SMPSs), which efficiently convert
alternating to direct current (AC to DC) and step-line voltages of 110-120 V or 220-240 V down to the 12-, 5-,
3.3-V and lower levels needed by system components. These functions are typical for consumer electronics and
data centers, but SMPSs are also used for DC-to-DC conversion, and for higher voltage levels in inverters for
renewable energy, as well as in automotive electronics, industrial equipments and other types of high-power
systems.
Figure 1 shows the flow of a generalized SMPS. An input voltage, often AC at a high voltage and
low frequency, is
rectified to DC. Line filters serve to block the high frequencies developed in the power supply from
transmitting back on the source line. A high-frequency power switch-the heart of the SMPS-converts the DC signal
to a pulsed voltage waveform. The output from the switch is transformed to the needed voltage and filtered for a
steady output at the level required by the low-voltage system. Feedback from the output is used by a controller
to supply pulse-width-modulated
(PWM) signals to the driver for the power switch, providing regulation. The pulse width of the signal is
increased or decreased as load requirements change.
Figure 1: Generic functions of a switched-mode power
supply.
Traditionally, power switches have been silicon MOSFETs (metal-on-silicon field-effect transistors), but are now
being replaced by GaN FETs.
Depending on system requirements, a wide variety of design topologies can be used and will require various
arrangements of power switches, from single-FET boost converters, through a number of two-FET designs, up to
four-FET full-bridge converters. The switch and its driver form an extremely sensitive area of the design as
they must perform precisely as the controller is commanding. If they do not, the power system becomes unstable.
Additionally, because of rapid rise and fall times of the modulated voltages, noise can be injected to the
feedback loop that may result in an unstable power system.
One requirement for all grid-connected systems is isolation between what comes from the grid and what is supplied
to the system, providing safety for the downstream equipment. Another concern is that high-frequency operation
of the power conversion must not be allowed to interfere with power delivered by the grid and create noise on
the source power line. GaN devices address this isolation requirement and need to reduce electromagnetic
interference by allowing higher frequency operation. This higher frequency can reduce the size of the isolation
transformer and input filter.
Advantages of GaN for SMPS systems
GaN has important advantages over silicon for power supply switching because it offers lower losses at higher
voltages. It also uses less energy to turn on and off. Si switches have improved greatly over the years, but for
the same size and high voltage, GaN offers a significant improvement that is unlikely to be matched by Si.
Today, Si MOSFETs have a sizeable cost advantage over GaN, but over time that cost differential will be reduced.
GaN switching devices are offered over a wide range of operating voltages. They offer power designers the
opportunity to reduce the physical size of their solution by operating at higher switching frequencies while
maintaining desired efficiencies for a very large range of input and output voltages. Applications where GaN is
most valuable tend to be those where the power solution needs to be miniaturized as much as possible.
Figure 2 shows the basic structure of a GaN transistor. As discussed earlier, the GaN material
is on a Si
substrate. By doing this we get the advantage of the decades of Si processing while we also get the advantage of
GaN. One benefit comes from the higher band gap voltage.
Figure 2: Cross section of an enhancement mode GaN
FET.
Semiconductors exist as a class of materials because of band gap energy-the jump in voltage required to change
the material from an insulator to a conductor. The band gap energy of 3.2 electron-volts (eV) that GaN offers is
nearly three times that of Si. Theoretically, this higher band gap means better performance at higher
temperatures, because more heat can be sustained before the substance becomes conductive. In the future, this
feature may improve GaN performance in automotive, industrial and other high-temperature environments.
The GaN learning curve in SMPS design
For the many advantages GaN offers, the technology is just beginning to find its way into power supply design.
Previous uses of GaN in LEDs and wireless applications might give the impression that the technology was ready
for power supplies, too. But, in fact, significant process and device development was required to use GaN in
power FETs and have slowed product development. Moreover, differences in new FETs from their Si predecessors
have compelled IC suppliers and system designers to proceed carefully, resolving design complexities issue by
issue. Traditional GaN devices are normally on, or in depletion mode, whereas Si MOSFETs are enhancement- mode
devices that are normally off. In order to provide drop-in replacements for Si MOSFETs, GaN FET switch suppliers
either redesigned their products to operate in enhancement mode or used another switch in series to provide the
normally off functionality.
Replacing a Si MOSFET with a GaN FET is only the beginning of the redesign. The higher frequency capability of a
GaN transistor demands greater timing precision in the switch driving signal, and the switches are highly
sensitive to parasitic impedances from packages, interconnect and outside sources. Integrated Si-based GaN
drivers that turn GaN switches on and off at high speeds have helped move GaN-enabled SMPS design along. Mature
Si processes enable the development of these extremely precise, high-frequency tunable drivers. For example,
TI's LM5113 gate driver was created to control high- and low-side enhancement-mode GaN power switches at medium
voltage levels. The gate driver integrates the required components to optimize the performance of GaN switches.
This integration not only reduces board space but also helps simplify the design. In addition to achieving
high-precision drive timing with minimal delay, the device also provides important protections for the
efficient, precise operation of the GaN switch. For example, bootstrap clamping keeps the gate-to-source voltage
in a safe operating area; a high-current pull-down improves dv/dt immunity and prevents accidental activation of
the low side; independent source and sink pins allow optimization of turn-on and turn-off times for efficiency
and low noise; and fast propagation delay matching optimizes dead times when the switch is in transition.
System-level solutions for GaN-based SMPS design
Combined in use with fast, precise power management control, GaN gate drivers have considerably advanced
GaN-based SMPS design. However, the gate drivers by themselves are limited in how much optimization they can
offer. Even the shortest possible traces between the driver and the GaN switch give rise to delays that vary
according to the design.
Future IC solutions will need to control variability issues resulting from the layout and design of passive
components, since these are all-important in coupling the driver and switch. Because the
two devices are based on different materials with widely different properties, they probably will not be
integrated economically in a single chip (die)
in the near future. However, a single-package module (Figure 3) that integrates the FETs,
driver and passive
devices supporting the switch would considerably reduce the area and component count of the SMPS. This size
reduction would also mean a reduction in system manufacturing costs, along with the increased efficiency of
GaN-based design.
Just as important as scaling down the solution is decreasing design complexity. A driver-switch module would
reduce inter-chip connections to the shortest possible lengths, minimizing the delay times and parasitic
impedances that serve to distort the pulsed output of the switch. A well-designed module could reduce the
parasitic factors of a multi-chip design considerably, some of them by an order of magnitude or more.
Figure 3: Integrated GaN switch-gate driver module.
Another important factor in supplying system-level solutions is the controller-regulator, which has to operate at
the higher frequencies enabled by GaN. This device must respond to changes in the output voltages in real time.
The time resolution must also meet the precise pulse width requirements to minimize conduction losses during the
dead time. Fortunately, digital power controllers are available to support these requirements, offering
additional performance and I/O functions that can be used elsewhere in the system. TI offers in-depth expertise
in digital power control, which combines with the company's power supply technology to provide system-level
solutions for GaN regulation and controlled switching.
Also needed are magnetics for GaN-based designs, since these components are still scaled for silicon-enabled
frequencies. TI collaborates with power supply manufacturers and GaN research institutions to continuously press
magnetics suppliers for these components, but much depends on the market. As GaN-based power component
availability and volume increases, magnetics suppliers will get volume requests from their customers to
introduce components scaled for the technology. Once these and other enabling factors are in place, the industry
will be able to leverage the benefits of GaN in many power supply applications.
GaN innovation for tomorrow's needs
The world's growing population and rising development create an ever-increasing demand for electricity, while
environmental issues increase the need to do more with less energy. As we try to address these needs, the world
will benefit from innovations that help us deliver, convert and consume electrical power more efficiently,
resulting in technologies that improve and enhance our lives.
GaN is one such innovation that promises to help us get more out of our energy resources by minimizing power
losses in electrical conversion. Rising to GaN's challenges, TI is leveraging its leadership in power and
commitment to research and development to create solutions that reduce the complications that arise with
high-frequency power conversion. These differentiated solutions will help to simplify design, save space and
reduce component counts while minimizing the signal delays and stray interferences that reduce efficient
operation.
As products appear that offer these advantages, SMPS developers will be able to design higher-performance systems
at a faster time-to-market. The success of these systems will push GaN into new application areas, both at the
high-power, industrial end of the scale and at the low-power, mass-market end. Modules and other key parts of
system-level solutions will help us realize the full potential that GaN technology offers in power supply
efficiency.