광전자공학

선택 이미지 부품 번호 제조업체 설명 데이터시트 구매 가능 정보 가격 (KRW) 수량에 따라 단가별로 테이블의 결과를 필터링합니다. 수량 RoHS
SparkFun LED 조명바 및 조명 스트립 The WS2812 (often referred to as a "NeoPixel") has become the standard for addressable LED projects and development board indicator lights. While it may look like a common 5050-sized (5mm x 5mm) SMD LED it's far more advanced. Housed inside the tiny 14재고 상태
최소: 1
배수: 1
SparkFun 광 센서 개발 툴 The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWIR) camera core. It ships preconfigured to operate as a plug-and-play UVC 1.0 USB thermal webcam that will work with standard 73재고 상태
최소: 1
배수: 1

SparkFun LED 조명 개발 툴 Do not look into the light. You know you want to but boy will you be sorry. 1W per channel RGB High Power LEDs in one aluminum backed package. These LEDs will blow you away. Light them up then put a coffee cup over the LED to keep your eyes from se 16재고 상태
17예상 2026-07-30
최소: 1
배수: 1

SparkFun 다중 색상 LED Ever hear of a thing called RGB? Red Green Blue? How about an RGB LED? These 5mm units have four pins - one for each color and a common cathode (the longest pin). Use this LED for three status indicators or pulse width modulate all three and get mi 177재고 상태
360예상 2026-06-23
최소: 1
배수: 1
SparkFun 포토다이오드 The BPW34 is a tiny general purpose PiN photodiode. This photodiode has a ton of uses one of which is to use it is a mini solar cell to power your project. The cell is sensitive to a wide range of light wavelengths (430-1100nm) so it should produc 35재고 상태
최소: 1
배수: 1
SparkFun 광 센서 개발 툴 A simple breakout PCB for the GP1A57HR photo interrupter (also known as a photogate photodiode or phototransistor). This PCB has three connections for PWR GND and Signal.When the gate is clear SIG will be high (>4.9V). When the gate is blocked b 429재고 상태
최소: 1
배수: 1

SparkFun 카메라 렌즈 This is the 6mm CS-mount wide angle lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module. The lens produces a 3MP picture in a 0.5in image format and is easily interchangeable using the thumb screw and adapter included wi 2재고 상태
최소: 1
배수: 1
없음
SparkFun OLED 디스플레이 및 액세서리 The SparkFun Qwiic OLED Display can display up to four lines of text and features 128x32 pixels in a compact 0.91-inch display. (diagonal) frame. As an OLED this display does not have a backlight layer (unlike LCDs); therefore it s thinner consu 110재고 상태
최소: 1
배수: 1

SparkFun 카메라 및 카메라 모듈 A first for the Raspberry Pi ecosystem: A 64MP camera module that matches the specs of smartphone cameras. The Arducam 64MP Camera Module puts a 64MP sensor with autofocus in the standard Raspberry Pi camera module form factor. Much like the other ca 4재고 상태
최소: 1
배수: 1
SparkFun 광 센서 개발 툴 Built around the STHS34PF80 sensor from STMicroelectronics this board is designed to give engineers the ability to easily experiment and develop applications with the sensor. The board measures 1" x 1" and includes two Qwiic sensors four mounting h 38재고 상태
최소: 1
배수: 1
SparkFun 광 센서 개발 툴 The SparkFun Qwiic Mini Tristimulus Color Sensor is built around the OPT4048 High-Speed High Precision Tristimulus XYZ Color Sensor from Texas Instruments. This Mini Sensor features a single-chip high-resolution color sensor capable of measuring four 20재고 상태
20예상 2026-06-22
최소: 1
배수: 1

SparkFun 광 센서 개발 툴 The SparkFun Qwiic Mini Human Presence and Motion Sensor is built around the STHS34PF80 Low-power high-sensitivity infrared (IR) sensor for presence and motion detection from STMicroelectronics. This sensor features an infrared motion and presence d 26재고 상태
최소: 1
배수: 1
SparkFun LED 조명 개발 툴 The PicoBuck LED Driver is an economical and easy to use driver that will allow you to control and blend three different LEDs on three different channels. By default each channel is driven at 330mA; that current can be reduced by either presenting a 109재고 상태
최소: 1
배수: 1

SparkFun LED 조명 개발 툴 This is the FemtoBuck a small-size single-output constant current LED driver. Each FemtoBuck has the capability to dim a single high-power channel of LEDs from 0-350mA at up to 36V while the dimming control can be either accessed via PWM or analog s 193재고 상태
최소: 1
배수: 1

SparkFun 열화상 카메라 The PureThermal Mini Pro JST-SR is a powerful hackable thermal camera development kit designed for the FLIR Lepton thermal imaging core. This board combines plug-and-play simplicity with the advanced embeddable features that developers need. This k 3재고 상태
10주문 중
최소: 1
배수: 1
SparkFun 광 센서 개발 툴 Ambient Light Sensor B/O TEMT6000 70재고 상태
최소: 1
배수: 1

SparkFun LED 조명 개발 툴 The SparkFun Qwiic LED Stick features ten addressable APA102 LEDs making it easy to add full color LED control using I2C. Write to individual LEDs to display a count in binary or write to the whole strip for cool lighting effects. You can even add 68재고 상태
최소: 1
배수: 1
SparkFun LED 디스플레이 및 액세서리 We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These green 14-segment displays allow you to show off all sorts o 10재고 상태
최소: 1
배수: 1

SparkFun LED 디스플레이 및 액세서리 We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These 14-segment displays allow you to show off all sorts of numb 4재고 상태
10주문 중
최소: 1
배수: 1

SparkFun LED 디스플레이 및 액세서리 We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These pink 14-segment displays allow you to show off all sorts of 7재고 상태
최소: 1
배수: 1

SparkFun LED 디스플레이 및 액세서리 We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These red 14-segment displays allow you to show off all sorts of 6재고 상태
최소: 1
배수: 1

SparkFun 광 센서 개발 툴 This version of the QRE1113 breakout board features a digital output using a capacitor discharge circuit to measure the amount of reflection. This tiny board is perfect for line sensing when only digital I/O is available and can be used in both 3.3 44재고 상태
최소: 1
배수: 1

SparkFun 광 센서 개발 툴 RGB Light Sensor - ISL29125 39재고 상태
최소: 1
배수: 1

SparkFun 광 센서 개발 툴 SparkFun Spectr Sens Breakout AS7263 NIR 8재고 상태
156주문 중
최소: 1
배수: 1

SparkFun 카메라 및 카메라 모듈 Based on the 16MP Sony IMX519 sensor the Arducam Camera Module V3 with Autofocus provides Raspberry Pi users with all the power needed to build future-proof projects. Boasting twice the resolution of the V2 (16MP with the V3) its standout feature i 6재고 상태
최소: 1
배수: 1